CC2650STK
SimpleLink SensorTag
CC2650STK
概述
全新的 SensorTag IoT 套件可帮您实现自己的云连接产品创意。现新推出的 SensorTag 包含 10 个采用微型红色封装的低功耗 MEMS 传感器。它可通过 DevPack 实现扩展,因此易于添加您的传感器或传动器。
通过低功耗蓝牙连接到云,在 3 分钟内在线获得传感器数据。SensorTag 开箱即可使用,带有 iOS 和 Android 应用,无需编程经验即可开始操作。
全新的 SensorTag 基于 CC2650 无线 MCU,功耗比此前的低功耗蓝牙产品低 75%。因此,SensorTag 可由电池供电,而且一个纽扣电池可以工作多年。
低功耗蓝牙 SensorTag 包含 iBeacon 技术。因此,您的手机可根据 SensorTag 数据和物理位置启动应用程序并自定义内容。
此外,可通过 ZigBee®/6LoWPAN 技术启用 SensorTag。
特性
- 更多传感器!
- 为更多低功耗传感器添加支持
- 10 个传感器,支持光、数字麦克风、磁传感器、湿度、压力、加速计、陀螺仪、磁力计、物体温度以及环境温度
- 功耗更低
- 纽扣电池寿命更长,实现无电池应用
- 高性能 ARM Cortex M3 (CC2650)
- 云连接
- 从任意地点访问和控制您的 SensorTag
- 与移动应用无缝集成
- DevPack 让您可以按照自己的设计扩展 SensorTag
- 所有 SensorTag 类型之间均可互换
- 完整的开发系统
- 使用 15 美元的调试 DevPack 即可扩展
- 包括 Code Composer Studio 编译器许可证
- 具有出色的灵活性,适用于物联网应用
- 通过固件升级,支持 ZigBee 或 6LoWPAN
- 与具有 352kB 闪存和 80kB SRAM 的 SimpleLink Arm® Cortex®-M4F CC2642R 和 CC2652R 低功耗蓝牙/多协议 2.4GHz 无线 MCU 引脚对引脚兼容
- Simplelink Bluetooth low energy SensorTag featuring the CC2650 wireless MCU
- CR2032 battery
- Quick Start Guide
- iOS and Android app, downloadable from App Store and Google Play
立即订购并开发
CC2650STK — SimpleLink SensorTag
FLASH-PROGRAMMER-2 — SmartRF 闪存编程器 v2
Zip file with Windows Installer and SW Manifest
产品
低功耗 2.4GHz 产品
Sub-1GHz 无线 MCU
其他无线产品
汽车类无线连接产品
硬件开发
评估板
开发套件
文档
Compressed source file archive
发布信息
SmartRF Flash Programmer 2 can be used to program the flash memory in Texas Instruments ARM based low-power RF wireless MCUs over the debug and serial interfaces. The flash programmer includes both a graphical user interface and a command line interface.
最新信息
- Support for the CC2640R2L added.
- Updated emupack to version 9.2.0.00002.
BLE-STACK-2-X — BLE-STACK V2.2(支持 CC2640/CC2650)
Windows Installer for Simplelink BLE 2 x SDK
Link to Windows Installer for Code Composer Studio IDE
产品
低功耗 2.4GHz 产品
硬件开发
评估板
开发套件
文档
Archive Installers for Simplelink BLE 2 x SDK
发布信息
This is version 2.2.7 of the TI Bluetooth® low energy protocol stack Software Development Kit (SDK). The BLE-Stack SDK allows for the development of single-mode Bluetooth low energy (BLE) applications on TI's first generation SimpleLink Bluetooth low energy CC2640 and Multi-Standard CC2650 wireless microcontroller units (MCUs) supporting version 5.1 of the Bluetooth specification with features defined by version 4.2 of the Bluetooth specification. The CC26x0 family of wireless MCUs includes a 32-bit Arm® Cortex™-M3 as the main application CPU running at 48 MHz, a dedicated Cortex-M0 processor for the radio / Physical Layer (PHY), and an autonomous Sensor Controller Engine for low-power sensing applications. The BLE protocol stack is built on top of the TI Real-time Operating System (TI-RTOS) which provides advanced power management and flexible peripheral driver capabilities allowing the development of highly optimized and power efficient standalone or network processor applications. The TI-RTOS SDK is installed during the BLE-Stack SDK installation.
Version 2.2.7 of the BLE-Stack is a maintenance update to TI's existing royalty-free Bluetooth low energy software protocol stack which is certified for Bluetooth specification version 5.1. This release includes support for all core specification version 4.2 Low Energy (LE) features as well as several development kits. This protocol stack update is in addition to support of all major Bluetooth LE core specification version 4.1 features, including support for up to 8 master or slave BLE connections. Please note that no Bluetooth 5 or Bluetooth 5.1 features are supported. A few examples of what can be created using the sample applications in this SDK and/or the additional resources found in the Examples section below include Bluetooth beacons incorporating the popular Apple iBeacon® and Eddystone™ formats, glucose, heart rate and fitness monitors, dongles for cable replacement via a BLE Serial Port Bridge and industrial motor monitors.
See What's New section for an overview of the changes included in this release. The Bluetooth core specification version 4.2 features supported in this release allow development of the most secure and power efficient products incorporating the Bluetooth low energy specification.
最新信息
- [Errata 17113] Impersonation the Passkey Entry Protocol -- do not except the same x coordinate of the public key during pairing.
- Impersonation the Passkey Entry Protocol -- exclude debug keys from rejection of mirror attack.
SMARTRF-STUDIO-7 — SmartRF Studio
产品
MSP430 微控制器
低功耗 2.4GHz 产品
Sub-1GHz 无线 MCU
Sub-1GHz 收发器
其他无线产品
汽车类无线连接产品
硬件开发
开发套件
评估板
接口适配器
子卡
文档
SmartRF Studio 7 in Cloud TI Resource Explorer
Compressed source file archive
发布信息
SmartRF™ Studio is a Windows application that can be used to evaluate and configure Low Power RF devices from Texas Instruments. The application helps designers of RF systems to easily evaluate the radio at an early stage in the design process. It is especially useful for generation of configuration register values and commands, and for practical testing and debugging of the RF system. SmartRF Studio can be used either as a standalone application or together with applicable evaluation boards or debug probes for the RF device.
最新信息
- Updated RF PHY settings for the CC13x4/CC26x4 devices
- Various improvements and bug-fixes
SWRC306 — Build Your Own Dev Pack
SWRC306 — Build Your Own Dev Pack
硬件开发
开发套件
发布信息
SENSOR-CONTROLLER-STUDIO — Sensor Controller Studio
Installer executable
Compressed archive
产品
低功耗 2.4GHz 产品
Sub-1GHz 无线 MCU
其他无线产品
汽车类无线连接产品
硬件开发
开发套件
评估板
文档
HTML document
Compressed source file archive
发布信息
Sensor Controller Studio is used to write, test and debug code for the CC26xx/CC13xx Sensor Controller, allowing for ultra-low power application design.
The tool generates a Sensor Controller Interface driver, which is a set of C source files to be compiled into the System CPU (ARM Cortex-M3/M4) application. These source files contain the Sensor Controller firmware image and associated definitions, and generic functions that allow the System CPU application to control the Sensor Controller and exchange data.
The Sensor Controller is a small CPU core that is highly optimized for low power consumption and efficient peripheral operation. The Sensor Controller is located in the CC26xx/CC13xx auxiliary (AUX) power/clock domain, and can perform simple background tasks autonomously and independently of the System CPU and the MCU domain power state. Such tasks include but are not limited to:
- Analog sensor polling, using ADC or comparator
- Digital sensor polling, using SPI, I2C or other protocols
- Capacitive sensing, using current source, comparator and time-to-digital converter (TDC)
- Waveform generation, for example for LCDs
The Sensor Controller is user programmable, using a simple programming language with syntax similar to C. This allows for sensor polling and other tasks to be specified as sequential algorithms, rather than static configuration of complex peripheral modules, timers, DMA, register programmable state machines, event routing and so on. The main advantages are:
- Flexibility
- Dynamic reuse of hardware resources
- Ability to perform simple data processing without need for dedicated hardware
- Observability and debugging options
最新信息
- Added support for new devices: CC2672R3, CC2672P3, CC2662R-Q1, CC2652PSIP and CC2652P7.
- Added example support for new SDKs, using TI-RTOS 7 and GPIO driver for the latest CC13x2/CC26x2 SDK.
- Minor improvements.
- Bug-fixes.
SWRC258 — BLE Device Monitor (v2.9.0)
SWRC258 — BLE Device Monitor (v2.9.0)
产品
低功耗 2.4GHz 产品
汽车类无线连接产品
硬件开发
开发套件
发布信息
设计文件
技术文档
类型 | 标题 | 下载最新的英文版本 | 日期 | |||
---|---|---|---|---|---|---|
证书 | CC2650STK EU Declaration of Conformity (DoC) | 2019年 1月 2日 | ||||
产品概述 | SimpleLink Ultra-low power wireless microcontroller platform (Rev. B) | 2016年 10月 28日 | ||||
白皮书 | Bringing Wireless Scalability to Intelligent Sensing Applications (Rev. B) | 2016年 8月 25日 | ||||
更多文献资料 | Allegion Case Study (Rev. A) | 2016年 4月 12日 | ||||
白皮书 | A guide to SensorTag Hackathons: Resources | 2016年 3月 8日 | ||||
更多文献资料 | CC2650RC Quick Start User's Guide | 2016年 3月 8日 | ||||
更多文献资料 | CC2650 SensorTag Quick Start Guide (Rev. A) | 2016年 2月 16日 | ||||
技术文章 | Understanding wireless connectivity in industrial IoT applications | PDF | HTML | 2015年 8月 4日 | |||
技术文章 | 9 reference designs to help you get started in the IoT this summer | PDF | HTML | 2015年 7月 23日 | |||
电子书 | Understanding Wireless Connectivity in the Industrial IoT | 2015年 7月 22日 | ||||
技术文章 | Sweetzpot, a computational quest towards zen in the art of rowing | PDF | HTML | 2015年 7月 7日 | |||
产品概述 | SimpleLink Bluetooth Smart CC2640 Wireless Microcontroller | 2015年 2月 10日 | ||||
产品概述 | SimpleLink 6LoWPAN/ZigBee CC2630 Wireless Microcontroller | 2015年 2月 10日 |