Get started with capacitive touch applications with the CAPTIVATE-FR2676
Explore capacitive touch applications with CapTIVate™ MCU(s). This bundle includes beginner workshops, out-of the-box demos, and specific hardware for metal, phone, and self-capacitance touch designs.
评估板
CAPTIVATE-FR2676 — 电容式触控 MSP430FR2676 MCU 主板
TI.com 上无现货
硬件编程工具
CAPTIVATE-PGMR — MSP430 CapTIvate MCU 编程器
TI.com 上无现货
评估板
CAPTIVATE-BSWP — 电容式触控自电容按钮、滑块、滚轮和接近传感器演示板
TI.com 上无现货
评估板
CAPTIVATE-METAL — 适用于 CapTIvate™ 开发套件的触摸金属电容式传感附加电路板
Working with metal.
TI.com 上无现货
开发套件
CAPTIVATE-PHONE — 具有触觉反馈功能的电容式触控互电容传感器演示板
Wanting to simulate a touch application in a phone form factor.
TI.com 上无现货
应用软件和框架
MSPCAPTDSNCTR — MSP CapTIvate 设计中心 GUI
MSPCAPTDSNCTR — MSP CapTIvate 设计中心 GUI
版本: 1.83.00.08
发布日期: 16 五月 2020
Captivate Design Center for Windows
校验和
Captivate Design Center for Mac OS X
校验和
Captivate Design Center for Linux
校验和
产品
MSP430 微控制器
硬件开发
评估板
开发套件
硬件编程工具
文档
Release Notes
API Guide
Users Guide
发布信息
CapTIvate™ brings together an exciting new capacitive touch measurement technology, a powerful CapTIvate™ Design Center GUI, a versatile hardware development platform and a full feature capacitive touch software library, creating the next step in evolution for capacitive touch sensor design. The CapTIvate™ Design Center is a rapid development tool that accelerates capacitive touch designs for CapTIvate™ Technology enabled MSP430 devices. By helping guide the product developer through the capacitive touch development process, the CapTIvate™ Design Center can simplify and accelerate any touch design through the use of innovative user graphical interfaces, wizards and controls.
最新信息
- CapTIvate Technology Guide
- Add the Temperature Drift information in Design Guide section
- Update the Devices section with key sensing parameters and comparison between two generations
- Software Library
- Add the support for new devices MSP430FR2672 and MSP430FR2673
- Design Center
- Please re-create the projects created from the previous version to get all the new features.
- Added support for TrackPad sensors
- Minor bug fixes
软件编程工具
UNIFLASH — 适用于大多数 TI 微控制器 (MCU) 和毫米波传感器的 UniFlash
UNIFLASH — 适用于大多数 TI 微控制器 (MCU) 和毫米波传感器的 UniFlash
版本: 9.0.0
发布日期: 20 十二月 2024
校验和
校验和
校验和
产品
C2000 实时微控制器
基于 Arm 的处理器
Arm Cortex-M0+ MCU
Arm Cortex-R MCU
汽车毫米波雷达传感器
工业毫米波雷达传感器
发布信息
UniFlash is a standalone tool used to program on-chip and external flash memory on TI MCUs and on-board flash memory for Sitara processors. UniFlash has a GUI, command line, and scripting interface. UniFlash is available free of charge.
最新信息
- Device support sync-up with CCS v20.0.1
- C29 device family support, including flash programming support on C29 and M4 core
- xWRL68 Radar device family support with serial flash programming
- New CRC32 GUI option for Image Integrity check
- Updated the MSP Bootloader flash programming support
- added additional boards to the device selection list
- Remove the depreciated Blackhawk XDS560v1 debug probes from the list
- various bug fixes