BOOSTXL-CC2650MA
TI SimpleLink 低功耗 Bluetooth® CC2650 模块 BoosterPack 插件模块
BOOSTXL-CC2650MA
概述
通过CC2650 模块 BoosterPack 套件可以简便快捷地将蓝牙低能耗添加到您的 LaunchPad 中。只需将 CC2650 模块 BoosterPack 插入 MSP432 LaunchPad!
CC2650 模块 BoosterPack 是一款具备无线网络处理器软件的编程套件,可以让您通过简单的 UART 接口将蓝牙低能耗连接添加到任何应用。模块 Boosterpack 还包括 JTAG 连接,可对 CC2650 模块进行编程和调试。如此,您就可以在 CC2650 模块上开发任何蓝牙低能耗应用。
特性
- 蓝牙低能耗模块 BoosterPack 使用带有集成型天线的 CC2650 模块
- 与 MSP432 LaunchPad 兼容
- 经过预先认证的模块可快速推向市场
- 调试用于在模块上开发任何蓝牙低能耗应用的接口
- 1 x CC2650 Module BoosterPack
- 10-pin JTAG debug cable
- 1 x Additional CC2650 Module Sample
- To download the host code example running on MSP432 LaunchPad, please visit this page
低功耗 2.4GHz 产品
立即订购并开发
BOOSTXL-CC2650MA — TI SimpleLink 低功耗 Bluetooth® CC2650 模块 BoosterPack 插件模块
SIMPLELINK-SDK-BLUETOOTH-PLUGIN — SimpleLink™ MCU SDK 蓝牙插件
Windows Installer for SimpleLink SDK BLE Plugin
macOS Installer for SimpleLink SDK BLE Plugin
Linux Installer for SimpleLink SDK BLE Plugin
产品
Wi-Fi 产品
Arm Cortex-M4 MCU
低功耗 2.4GHz 产品
硬件开发
评估板
开发套件
文档
SimpleLink SDK BLE Plugin User's Guide
最新信息
- This version of the SimpleLink Bluetooth Plugin now enables a BLE two-chip solution to act as a GAP Central role. Previous versions of this plugin only included support for GAP Peripheral role. This new functionality is showcased through the addition of the new simple_central example, which uses the MSP432E401Y as the Host device and the CC26x2R1 as the NWP. The simple_central example demonstrates the following features:
- Host: MSP432E401Y
- NWP: CC26X2R1
- GAP Central role support
- Host Controller Interface (HCI) protocol used for communication with the NWP
- BLE5 support
- Power management
- Low Energy Secure Connection (LESC) Pairing
- Tested with up to 4 peripherals connected simultaneously (but can support more than 4 connections)
- Supports a subset of TI Vendor Specific HCI commands and Bluetooth LE HCI commands/events. More information on these APIs can be found BLE Vendor Specific API Guide.
- Works out-of-box with the Sensors BoosterPack and Project Zero examples that are also in the SimpleLink SDK Bluetooth Plugin.
- The GAP Central source code is also showcased in a separate downloadable: the SimpleLink BLE Plugin Azure Gateway Example Pack. This example pack demonstrates enabling a user’s BLE two-chip solution to become a gateway to the Azure IoT cloud. The SimpleLink BLE Plugin Azure Gateway Example Pack can be found on www.ti.com.
发布信息
The SimpleLink™ SDK BLE Plugin is a companion software package that enables the use of a Bluetooth radio on any standard MSP432P4 platform, MSP432E4 or CC32XX platform, and enables this two-chip solution to act as either a GAP Peripheral role or a GAP Central role. By having the ability to seamlessly and modularly add Bluetooth functionality (more specifically Bluetooth Low Energy/BLE) to an embedded system, a programmer can enable their embedded device to become a gateway to various IOT infrastructures.
For examples demonstrating the two-chip solution in a peripheral role, the plugin leverages the use of the TI Simple Application Processor (SAP) driver connected to a CC26xx Simple Network Processor (SNP) to provide a highly customizable hardware configuration. For software connectivity between the SAP and the SNP, an architecture agnostic HAL/Drivers layer is used to promote software portability and maximize collateral reuse.
For examples demonstrating the two-chip solution in a central role, communication between the NWP and the Host occurs through a UART serial interface using the Host Controller Interface (HCI) protocol. TI Vendor Specific HCI commands and a limited subset of Bluetooth LE HCI commands/events to implement a Bluetooth application. By using TI Vendor Specific commands and events, the application can communicate with and access the BLE stack.
BLE-STACK-2-X — BLE-STACK V2.2(支持 CC2640/CC2650)
产品
低功耗 2.4GHz 产品
硬件开发
评估板
开发套件
文档
Archive Installers for Simplelink BLE 2 x SDK
发布信息
This is version 2.2.8 of the TI Bluetooth® low energy protocol stack Software Development Kit (SDK). The BLE-Stack SDK allows for the development of single-mode Bluetooth low energy (BLE) applications on TI's first generation SimpleLink Bluetooth low energy CC2640 and Multi-Standard CC2650 wireless microcontroller units (MCUs) supporting version 5.1 of the Bluetooth specification with features defined by version 4.2 of the Bluetooth specification. The CC26x0 family of wireless MCUs includes a 32-bit Arm® Cortex™-M3 as the main application CPU running at 48 MHz, a dedicated Cortex-M0 processor for the radio / Physical Layer (PHY), and an autonomous Sensor Controller Engine for low-power sensing applications. The BLE protocol stack is built on top of the TI Real-time Operating System (TI-RTOS) which provides advanced power management and flexible peripheral driver capabilities allowing the development of highly optimized and power efficient standalone or network processor applications. The TI-RTOS SDK is installed during the BLE-Stack SDK installation.
Version 2.2.8 of the BLE-Stack is a maintenance update to TI's existing royalty-free Bluetooth low energy software protocol stack which is certified for Bluetooth specification version 5.1. This release includes support for all core specification version 4.2 Low Energy (LE) features as well as several development kits. This protocol stack update is in addition to support of all major Bluetooth LE core specification version 4.1 features, including support for up to 8 master or slave BLE connections. Please note that no Bluetooth 5 or Bluetooth 5.1 features are supported. A few examples of what can be created using the sample applications in this SDK and/or the additional resources found in the Examples section below include Bluetooth beacons incorporating the popular Apple iBeacon® and Eddystone™ formats, glucose, heart rate and fitness monitors, dongles for cable replacement via a BLE Serial Port Bridge and industrial motor monitors.
See What's New section for an overview of the changes included in this release. The Bluetooth core specification version 4.2 features supported in this release allow development of the most secure and power efficient products incorporating the Bluetooth low energy specification.
最新信息
- [PSIRT-129] The generate key functions (ECCROMCC26XX_genKeys, and ECC_generateKey) shall now validate the ECC key pair
CC26XX-REPORTS — CC26xx 监管认证报告
产品
低功耗 2.4GHz 产品
硬件开发
评估板
文档
Link to FCC, ISED, CE, & Japan Certification Reports
Link to FCC, ISED, CE, & UK, Japan, Korea, and Taiwan Certification Reports
Link to FCC, ISED, CE, & UK Certification Reports
Link to FCC, ISED, CE, & UK Certification Reports
Link to CC3230x-CC26x2EM-7ID Reference-Only CE & FCC Certification Reports
发布信息
This page provides access to the CC26XX certification reports. Here you will find certification reports for both modules and EVMs. Note that module certification reports can be reused by the customer for regulatory compliance. However the customer should consult with their regulatory house to ensure they meet the requirements for certification at their product level. EVM certification reports are provided for reference only. When using a chip down version, the customer is responsible for their own certification.
最新信息
- Updated CC2651R3SIPAT0MOUR with Japan, Korea, and Tiawan reports
- Updated CC2652RSIPMOT CE with missing safety report
设计文件
技术文档
类型 | 标题 | 下载最新的英文版本 | 日期 | |||
---|---|---|---|---|---|---|
* | 用户指南 | CC2650 Module BoosterPack™ Getting Started Guide (Rev. A) | 2016年 6月 29日 | |||
证书 | BOOSTXL-CC2650MA EU Declaration of Conformity (DoC) | 2019年 1月 2日 | ||||
电子书 | TI-RSLK modules 1 - 20 (Rev. A) | 2018年 5月 30日 | ||||
更多文献资料 | 简介:传感器集成 | 2017年 11月 17日 | ||||
更多文献资料 | 实验室:传感器集成 | 2017年 11月 17日 | ||||
更多文献资料 | Jacki Project Lecture | 2017年 11月 17日 | ||||
应用手册 | Running Standalone Bluetooth® low energy Applications on CC2650 Module (Rev. A) | PDF | HTML | 2017年 6月 7日 | |||
应用手册 | Running Standalone Bluetooth® low energy Applications on CC2650 Module | 2017年 1月 18日 |